task.
h
char *pcTaskGetTaskName( TaskHandle_t xTaskToQuery );
- Returns
- The text (human readable) name of the task referenced by the handle xTaskToQuery. A task can query its own name by either passing in its own handle, or by setting xTaskToQuery to NULL. INCLUDE_pcTaskGetTaskName must be set to 1 in FreeRTOSConfig.h for pcTaskGetTaskName() to be available.
h
signed char *pcTaskGetTaskName( xTaskHandle xTaskToQuery );
- Returns
- The text (human readable) name of the task referenced by the handle xTaskToQueury. A task can query its own name by either passing in its own handle, or by setting xTaskToQuery to NULL. INCLUDE_pcTaskGetTaskName must be set to 1 in FreeRTOSConfig.h for pcTaskGetTaskName() to be available.