This simple example shows how to set up a collection of spinners and display them on the screen.
All SAM devices can be used. This example has been tested with the following setup:
This example application will initialize string spinner and two integer spinners, set up a spin collection with the spinners and display them on the screen.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR. Other compilers may or may not work.
For further information, visit Microchip.