Microchip® Advanced Software Framework

Extra Information for I2S Driver

Acronyms

Below is a table listing the acronyms used in this module, along with their intended meanings.

Acronym Description
I2S, IIS Inter-IC Sound Controller
MCK Master Clock
SCK Serial Clock
FS Frame Sync
SD Serial Data
ADC Analog-to-Digital Converter
DAC Digital-to-Analog Converter
TDM Time Division Multiplexed
PDM Pulse Density Modulation
LSB Least Significant Bit
MSB Most Significant Bit
DSP Digital Signal Processor

Dependencies

This driver has the following dependencies:

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Initial Release