Microchip® Advanced Software Framework

Extra Information for SERCOM SPI Master Driver w/ Vectored I/O

Acronyms

The table below presents the acronyms used in this module.

Acronym Description
GCLK Generic Clock
MISO Master Input, Slave Output
MOSI Master Output, Slave Input
SCK Serial Clock
SPI Serial Peripheral Interface
SS Slave Select

Dependencies

This driver has the following dependencies:

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Initial Release