thirdparty
wireless
avr2130_lwmesh
source
phy
at86rf212
inc
Data Structures
at86rf212/inc/phy.h File Reference
#include <stdint.h>
#include <stdbool.h>
Data Structures
struct
PHY_DataInd_t
#define
PHY_RSSI_BASE_VAL_BPSK_20
(-100)
#define
PHY_RSSI_BASE_VAL_BPSK_40
(-99)
#define
PHY_RSSI_BASE_VAL_OQPSK_SIN_RC_100
(-98)
#define
PHY_RSSI_BASE_VAL_OQPSK_SIN_250
(-97)
#define
PHY_RSSI_BASE_VAL_OQPSK_RC_250
(-97)
#define
PHY_HAS_RANDOM_NUMBER_GENERATOR
#define
PHY_HAS_AES_MODULE
enum
{
PHY_STATUS_SUCCESS
= 0,
PHY_STATUS_CHANNEL_ACCESS_FAILURE
= 1,
PHY_STATUS_NO_ACK
= 2,
PHY_STATUS_ERROR
= 3
}
typedef struct
PHY_DataInd_t
PHY_DataInd_t
void
PHY_Init
(void)
void
PHY_SetRxState
(
bool
rx)
void
PHY_SetChannel
(uint8_t
channel
)
void
PHY_SetBand
(uint8_t band)
void
PHY_SetModulation
(uint8_t modulation)
void
PHY_SetPanId
(uint16_t panId)
void
PHY_SetShortAddr
(uint16_t
addr
)
void
PHY_Sleep
(void)
void
PHY_Wakeup
(void)
void
PHY_DataReq
(uint8_t *
data
)
void
PHY_DataConf
(uint8_t
status
)
void
PHY_DataInd
(
PHY_DataInd_t
*ind)
void
PHY_TaskHandler
(void)
void
PHY_SetIEEEAddr
(uint8_t *ieee_addr)
uint16_t
PHY_RandomReq
(void)
void
PHY_EncryptReq
(uint8_t *text, uint8_t *
key
)
Generated on Fri Mar 4 2022 23:26:13 for SAMD21 by
1.8.5