Microchip® Advanced Software Framework

at86rf231/src/tal_pib.c File Reference
#include <stdint.h>
#include <string.h>
#include <stdbool.h>
#include <stdlib.h>
#include "pal.h"
#include "return_val.h"
#include "tal.h"
#include "ieee_const.h"
#include "tal_constants.h"
#include "tal_pib.h"
#include "at86rf231.h"
#include "tal_internal.h"

Functions

uint8_t convert_phyTransmitPower_to_reg_value (uint8_t phyTransmitPower_value)
 Converts a phyTransmitPower value to a register value. More...
 
 FLASH_DECLARE (int8_t tx_pwr_table[16])
 
void init_tal_pib (void)
 Initialize the TAL PIB. More...
 
static uint8_t limit_tx_pwr (uint8_t curr_transmit_power)
 Limit the phyTransmitPower to the trx limits. More...
 
retval_t tal_pib_get (uint8_t attribute, uint8_t *value)
 Gets a TAL PIB attribute. More...
 
retval_t tal_pib_set (uint8_t attribute, pib_value_t *value)
 Sets a TAL PIB attribute. More...
 
void write_all_tal_pib_to_trx (void)
 Write all shadow PIB variables to the transceiver. More...