Microchip® Advanced Software Framework

frame802154_t Struct Reference

Parameters used by the frame802154_create() function.

These parameters are used in the 802.15.4 frame header. See the 802.15.4 specification for details.

#include <frame802154.h>

Data Fields

frame802154_aux_hdr_t aux_hdr
 Aux security header. More...
 
uint8_t dest_addr [8]
 Destination address. More...
 
uint16_t dest_pid
 Destination PAN ID. More...
 
frame802154_fcf_t fcf
 Frame control field. More...
 
uint8_t * payload
 Pointer to 802.15.4 frame payload. More...
 
int payload_len
 Length of payload field. More...
 
uint8_t seq
 Sequence number. More...
 
uint8_t src_addr [8]
 Source address. More...
 
uint16_t src_pid
 Source PAN ID. More...