Microchip® Advanced Software Framework

mcps_data_ind_tag Struct Reference

This is the MCPS-DATA.indication message structure.

#include <mac_msg_type_data_ind.h>

Data Fields

enum msg_code cmdcode
 < This identifies the message as MCPS_DATA_INDICATION More...
 
uint8_t DSN
 The DSN of the received data frame. More...
 
uint64_t DstAddr
 The individual device address of the entity to which the MSDU is being transferred. More...
 
uint8_t DstAddrMode
 The destination addressing mode for this primitive corresponding to the received MPDU. More...
 
uint16_t DstPANId
 The 16 bit PAN identifier of the entity to which the MSDU is being transferred. More...
 
uint8_t mpduLinkQuality
 LQI value measured during reception of the MPDU. More...
 
uint8_t * msdu
 The set of octets forming the MSDU being indicated by the MAC sublayer entity. More...
 
uint8_t msduLength
 The number of octets contained in the MSDU being indicated by the MAC sublayer entity. More...
 
uint64_t SrcAddr
 The individual device address of the entity from which the MSDU was received. More...
 
uint8_t SrcAddrMode
 The source addressing mode for this primitive corresponding to the received MPDU. More...
 
uint16_t SrcPANId
 The 16 bit PAN identifier of the entity from which the MSDU was received. More...
 
uint32_t Timestamp
 Optional. More...