This is the MCPS-DATA.request message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
< This identifies the message as MCPS_DATA_REQUEST More... | |
uint64_t | DstAddr |
The individual device address of the entity to which the MSDU is being transferred. More... | |
uint8_t | DstAddrMode |
The destination addressing mode for this primitive and subsequent MPDU. More... | |
uint16_t | DstPANId |
The 16 bit PAN identifier of the entity to which the MSDU is being transferred. More... | |
uint8_t * | msdu |
The set of octets forming the MSDU to be transmitted by the MAC sublayer entity. More... | |
uint8_t | msduHandle |
The handle associated with the MSDU to be transmitted by the MAC sublayer entity. More... | |
uint8_t | msduLength |
The number of octets contained in the MSDU to be transmitted by the MAC sublayer entity. More... | |
uint8_t | SrcAddrMode |
The source addressing mode for this primitive and subsequent MPDU. More... | |
uint8_t | TxOptions |
The transmission options for this MSDU. More... | |