This is the MCPS-PURGE.confirm message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
< This identifies the message as MCPS_PURGE_CONFIRM More... | |
uint8_t | msduHandle |
The handle of the MSDU requested to be purge from the transaction queue. More... | |
uint8_t | status |
The status of the request to be purged an MSDU from the transaction queue. More... | |