Microchip® Advanced Software Framework

mlme_associate_conf_tag Struct Reference

This is the MLME-ASSOCIATE.confirm message structure.

#include <mac_msg_types.h>

Data Fields

uint16_t AssocShortAddress
 The short device address allocated by the coordinator on successful association. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_ASSOCIATE_CONFIRM. More...
 
uint8_t status
 The status of the association attempt. More...