Microchip® Advanced Software Framework

mlme_associate_ind_tag Struct Reference

This is the MLME-ASSOCIATE.indication message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t CapabilityInformation
 The operational capabilities of the device requesting association. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_ASSOCIATE_INDICATION. More...
 
uint64_t DeviceAddress
 The address of the device requesting association. More...