Microchip® Advanced Software Framework

mlme_associate_req_tag Struct Reference

This is the MLME-ASSOCIATE.request message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t CapabilityInformation
 Specifies the operational capabilities of the associating device. More...
 
uint8_t ChannelPage
 The channel page on which to attempt association. More...
 
enum msg_code cmdcode
 < This identifies the message as MLME_ASSOCIATE_REQUEST More...
 
address_field_t CoordAddress
 The address of the coordinator with which to associate. More...
 
uint8_t CoordAddrMode
 The coordinator addressing mode for this primitive and subsequent MPDU. More...
 
uint16_t CoordPANId
 The identifier of the PAN with which to associate. More...
 
uint8_t LogicalChannel
 The logical channel on which to attempt association. More...