This is the MLME-DISASSOCIATE.indication message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
This identifies the message as MLME_DISASSOCIATE_INDICATION. More... | |
uint64_t | DeviceAddress |
The address of the device requesting disassociation. More... | |
uint8_t | DisassociateReason |
The reason for the disassociation (see 7.3.1.3.2). More... | |