This is the MLME-DISASSOCIATE.request message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
This identifies the message as MLME_DISASSOCIATE_REQUEST. More... | |
uint64_t | DeviceAddress |
The address of the device to which to send the disassociation notification command. More... | |
uint8_t | DeviceAddrMode |
The addressing mode of the device to which to send the disassociation notification command. More... | |
uint16_t | DevicePANId |
The PAN identifier of the device to which to send the disassociation notification command. More... | |
uint8_t | DisassociateReason |
The reason for the disassociation (see 7.3.1.3.2). More... | |
uint8_t | TxIndirect |
TRUE if the disassociation notification command is to be sent indirectly. More... | |