This is the MLME-GET.confirm message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
< This identifies the message as MLME_GET_CONFIRM More... | |
uint8_t | PIBAttribute |
pib_value_t | PIBAttributeValue |
< The value of the indicated MAC PIB attribute that was read. More... | |
uint8_t | status |
The identifier of the MAC PIB attribute to get. More... | |