Microchip® Advanced Software Framework

mlme_poll_req_tag Struct Reference

This is the MLME-POLL.request message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 This identifies the message as MLME_POLL_REQUEST. More...
 
uint64_t CoordAddress
 The address of the coordinator to which the poll is intended. More...
 
uint8_t CoordAddrMode
 The addressing mode of the coordinator to which the poll is intended. More...
 
uint16_t CoordPANId
 The PAN identifier of the coordinator to which the poll is intended. More...