This is the MLME-RESET.request message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
< This identifies the message as MLME_RESET_REQUEST More... | |
uint8_t | SetDefaultPIB |
If TRUE, the MAC sublayer is reset and all MAC PIB attributes are set to their default values. More... | |