This is the MLME-SCAN.request message structure.
#include <mac_msg_types.h>
Data Fields | |
uint8_t | ChannelPage |
The channel page on which to perform the scan. More... | |
enum msg_code | cmdcode |
This identifies the message as MLME_SCAN_REQUEST. More... | |
uint32_t | ScanChannels |
The 5 MSBs (b27, ... More... | |
uint8_t | ScanDuration |
A value used to calculate the length of time to spend scanning each channel for ED, active, and passive scans. More... | |
uint8_t | ScanType |
Indicates the type of scan performed: 0 x 00 = ED scan (FFD only). More... | |