Microchip® Advanced Software Framework

mlme_set_conf_tag Struct Reference

This is the MLME-SET.confirm message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 < This identifies the message as MLME_SET_CONFIRM More...
 
uint8_t PIBAttribute
 
uint8_t status
 The identifier of the MAC PIB attribute that was written. More...