Microchip® Advanced Software Framework

mlme_start_conf_tag Struct Reference

This is the MLME-START.confirm message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 This identifies the message as MLME_START_CONFIRM. More...
 
uint8_t status
 The result of the attempt to start using an updated superframe configuration. More...