Microchip® Advanced Software Framework

mlme_start_req_tag Struct Reference

This is the MLME-START.request message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t BatteryLifeExtension
 If this value is TRUE, the receiver of the beaconing device is disabled macBattLifeExtPeriods full backoff periods after the interframe spacing (IFS) period of the beacon frame. More...
 
uint8_t BeaconOrder
 How often the beacon is to be transmitted. More...
 
uint8_t ChannelPage
 The channel page on which to begin using the new superframe configuration. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_START_REQUEST. More...
 
uint8_t CoordRealignment
 TRUE if a coordinator realignment command is to be transmitted prior to changing the superframe configuration or FALSE otherwise. More...
 
uint8_t LogicalChannel
 The logical channel on which to start using the new superframe configuration. More...
 
uint8_t PANCoordinator
 If this value is TRUE, the device will become the PAN coordinator of a new PAN. More...
 
uint16_t PANId
 The PAN identifier to be used by the device. More...
 
uint8_t SuperframeOrder
 The length of the active portion of the superframe, including the beacon frame. More...