This is the MLME-SYNC.request message structure.
#include <mac_msg_types.h>
Data Fields | |
uint8_t | ChannelPage |
The channel page on which to attempt coordinator synchronization. More... | |
enum msg_code | cmdcode |
This identifies the message as MLME_SYNC_REQUEST. More... | |
uint8_t | LogicalChannel |
The logical channel on which to attempt coordinator synchronization. More... | |
bool | TrackBeacon |
TRUE if the MLME is to synchronize with the next beacon and attempt to track all future beacons. More... | |