Microchip® Advanced Software Framework

Todo List
Global create (void)
For phase 1 the addresses are all long. We'll need a mechanism in the rime attributes to tell the mac to use long or short for phase 2.
Global get_cur_lun (void)
Implement.
Global LWIP_NETIF_TX_SINGLE_PBUF
: TCP and IP-frag do not work with this, yet:
Global macIeeeAddress
numbering needs to alligned with other special speer attributes
Global ns_input (void)
if I sent a NS before him, I win
File snmp_structs.h
namespace prefixes
Global stream_state (U8 id)
Implement.
Global stream_stop (U8 id)
Implement.