USB device driver for Human Interface Device (HID) generic interface.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | udi_hid_generic_desc_t |
Interface descriptor structure for HID generic. More... | |
struct | udi_hid_generic_report_desc_t |
Report descriptor for HID generic. More... | |
Macros | |
USB Interface Descriptors | |
The following structures provide predefined USB interface descriptors. It must be used to define the final USB descriptors. | |
#define | UDI_HID_GENERIC_STRING_ID 0 |
By default no string associated to this interface. More... | |
#define | UDI_HID_GENERIC_DESC |
Content of HID generic interface descriptor for all speed. More... | |
Functions | |
USB Device Interface (UDI) for Human Interface Device (HID) Generic Class | |
Common APIs used by high level application to use this USB class. | |
bool | udi_hid_generic_send_report_in (uint8_t *data) |
Routine used to send a report to USB Host. More... | |
Variables | |
Interface with USB Device Core (UDC) | |
Structure required by UDC. | |
UDC_DESC_STORAGE udi_api_t | udi_api_hid_generic |
Global structure which contains standard UDI API for UDC. More... | |