This is the quick start guide for the USB device interface CDC module (UDI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases.
The use cases contain several code fragments. The code fragments in the steps for setup can be copied into a custom initialization function, while the steps for usage can be copied into, e.g., the main application function.
Basic Use Case
In this basic use case, the "USB CDC (Single Interface Device)" module is used with only one communication port. The "USB CDC (Composite Device)" module usage is described in Advanced use cases.
Setup Steps
Prerequisites
This module is based on USB device stack full interrupt driven, and supporting Sleep manager sleepmgr. For AVR and SAM3/4 devices the clk_group clock services is supported. For SAMD devices the SAM System Clock Management (SYSTEM CLOCK) Driver clock driver is supported.
The following procedure must be executed to setup the project correctly:
- Specify the clock configuration:
- XMEGA USB devices need 48MHz clock input.
XMEGA USB devices need CPU frequency higher than 12MHz.
You can use either an internal RC48MHz auto calibrated by Start of Frames or an external OSC.
- UC3 and SAM3/4 devices without USB high speed support need 48MHz clock input.
You must use a PLL and an external OSC.
- UC3 and SAM3/4 devices with USB high speed support need 12MHz clock input.
You must use an external OSC.
- UC3 devices with USBC hardware need CPU frequency higher than 25MHz.
- SAMD devices without USB high speed support need 48MHz clock input.
You should use DFLL with USBCRM.
- In conf_board.h, the define CONF_BOARD_USB_PORT must be added to enable USB lines. (Not mandatory for all boards)
- Enable interrupts
- Initialize the clock service
The usage of Sleep manager sleepmgr service is optional, but recommended to reduce power consumption:
- Initialize the sleep manager service
- Activate sleep mode when the application is in IDLE state
conf_clock.h examples with USB support.
for AVR and SAM3/4 devices, add to the initialization code:
For SAMD devices, add to the initialization code:
Add to the main IDLE loop:
Example code
Content of conf_usb.h:
#define USB_DEVICE_VENDOR_ID 0x03EB
#define USB_DEVICE_PRODUCT_ID 0xXXXX
#define USB_DEVICE_MAJOR_VERSION 1
#define USB_DEVICE_MINOR_VERSION 0
#define USB_DEVICE_POWER 100
#define USB_DEVICE_ATTR USB_CONFIG_ATTR_BUS_POWERED
Add to application C-file:
Workflow
- Ensure that conf_usb.h is available and contains the following configuration which is the main USB device configuration:
#define USB_DEVICE_VENDOR_ID 0x03EB // Type Word
#define USB_DEVICE_PRODUCT_ID 0xXXXX // Type Word
#define USB_DEVICE_MAJOR_VERSION 1 // Type Byte
#define USB_DEVICE_MINOR_VERSION 0 // Type Byte
#define USB_DEVICE_POWER 100 // Type 9-bits
#define USB_DEVICE_ATTR USB_CONFIG_ATTR_BUS_POWERED // Flags
- Call the USB device stack start function to enable stack and start USB:
-
- Note
- In case of USB dual roles (Device and Host) managed through USB OTG connector (USB ID pin), the call of udc_start() must be removed and replaced by uhc_start(). SeRefer to "AVR4950 section 6.1 Dual roles" for further information about dual roles.
Usage Steps
Example Code
Content of conf_usb.h:
#define UDI_CDC_ENABLE_EXT(port) my_callback_cdc_enable()
extern bool my_callback_cdc_enable(void);
#define UDI_CDC_DISABLE_EXT(port) my_callback_cdc_disable()
extern void my_callback_cdc_disable(void);
#define UDI_CDC_LOW_RATE
#define UDI_CDC_DEFAULT_RATE 115200
#define UDI_CDC_DEFAULT_STOPBITS CDC_STOP_BITS_1
#define UDI_CDC_DEFAULT_PARITY CDC_PAR_NONE
#define UDI_CDC_DEFAULT_DATABITS 8
Add to application C-file:
static bool my_flag_autorize_cdc_transfert = false;
bool my_callback_cdc_enable(void)
{
my_flag_autorize_cdc_transfert = true;
return true;
}
void my_callback_cdc_disable(void)
{
my_flag_autorize_cdc_transfert = false;
}
void task(void)
{
if (my_flag_autorize_cdc_transfert) {
}
}
Workflow
- Ensure that conf_usb.h is available and contains the following configuration, which is the USB device CDC configuration:
#define USB_DEVICE_SERIAL_NAME "12...EF" // Disk SN for CDC
- Note
- The USB serial number is mandatory when a CDC interface is used.
#define UDI_CDC_ENABLE_EXT(port) my_callback_cdc_enable()
extern bool my_callback_cdc_enable(void);
- Note
- After the device enumeration (detecting and identifying USB devices), the USB host starts the device configuration. When the USB CDC interface from the device is accepted by the host, the USB host enables this interface and the UDI_CDC_ENABLE_EXT() callback function is called and return true. Thus, when this event is received, the data transfer on CDC interface are authorized.
#define UDI_CDC_DISABLE_EXT(port) my_callback_cdc_disable()
extern void my_callback_cdc_disable(void);
- Note
- When the USB device is unplugged or is reset by the USB host, the USB interface is disabled and the UDI_CDC_DISABLE_EXT() callback function is called. Thus, the data transfer must be stopped on CDC interface.
-
- Note
- Define it when the transfer CDC Device to Host is a low rate (<512000 bauds) to reduce CDC buffers size.
#define UDI_CDC_DEFAULT_RATE 115200
#define UDI_CDC_DEFAULT_STOPBITS CDC_STOP_BITS_1
#define UDI_CDC_DEFAULT_PARITY CDC_PAR_NONE
#define UDI_CDC_DEFAULT_DATABITS 8
- Note
- Default configuration of communication port at startup.
- Send or wait data on CDC line:
Advanced Use Cases
For more advanced use of the UDI CDC module, see the following use cases: