Microchip® Advanced Software Framework

scan_result_list_t Union Reference

Union to force alignment of variable portion of scan confirm with wpan_pandescriptor_t.

In order to allow proper alignment of members of the PAN descriptor list in the scan confirm for non 8-bit platforms (such as ARM), the variable portion of scan confirm at the end of the primitive needs to be aligned to at list of wpan_pandescriptor_t. This has no impact for 8-bit platforms.

#include <mac_msg_types.h>

Data Fields

uint8_t ed_value [1]
 
wpan_pandescriptor_t wpan_pan_desc