Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an xTaskHandle variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 00:44:41 for lwIP TCP/IP Stack HTTP stats example using Netconn API for SAM4E-EK by 1.8.5