|
uint8_t | mac_get_pib_attribute_size (uint8_t pib_attribute_id) |
|
uint32_t | mac_ready_to_sleep (void) |
| Checks if the mac stack is ready to sleep. More...
|
|
void | usr_mcps_data_conf (uint8_t msduHandle, uint8_t status, uint32_t Timestamp) |
| Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.confirm. More...
|
|
void | usr_mcps_data_ind (wpan_addr_spec_t *SrcAddrSpec, wpan_addr_spec_t *DstAddrSpec, uint8_t msduLength, uint8_t *msdu, uint8_t mpduLinkQuality, uint8_t DSN, uint32_t Timestamp, uint8_t SecurityLevel, uint8_t KeyIdMode, uint8_t KeyIndex) |
| Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.indication. More...
|
|
void | usr_mcps_purge_conf (uint8_t msduHandle, uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MCPS-PURGE.confirm. More...
|
|
void | usr_mlme_associate_conf (uint16_t AssocShortAddress, uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.confirm. More...
|
|
void | usr_mlme_associate_ind (uint64_t DeviceAddress, uint8_t CapabilityInformation) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.indication. More...
|
|
void | usr_mlme_beacon_notify_ind (uint8_t BSN, wpan_pandescriptor_t *PANDescriptor, uint8_t PendAddrSpec, uint8_t *AddrList, uint8_t sduLength, uint8_t *sdu) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-BEACON-NOTIFY.indication. More...
|
|
void | usr_mlme_comm_status_ind (wpan_addr_spec_t *SrcAddrSpec, wpan_addr_spec_t *DstAddrSpec, uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-COMM-STATUS.indication. More...
|
|
void | usr_mlme_disassociate_conf (uint8_t status, wpan_addr_spec_t *DeviceAddrSpec) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.confirm. More...
|
|
void | usr_mlme_disassociate_ind (uint64_t DeviceAddress, uint8_t DisassociateReason) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.indication. More...
|
|
void | usr_mlme_get_conf (uint8_t status, uint8_t PIBAttribute, void *PIBAttributeValue) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-GET.confirm. More...
|
|
void | usr_mlme_gts_conf (gts_char_t GtsChar, uint8_t status) |
|
void | usr_mlme_gts_ind (uint16_t DeviceAddr, gts_char_t GtsChar) |
|
void | usr_mlme_orphan_ind (uint64_t OrphanAddress) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-ORPHAN.indication. More...
|
|
void | usr_mlme_poll_conf (uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-POLL.confirm. More...
|
|
void | usr_mlme_reset_conf (uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-RESET.confirm. More...
|
|
void | usr_mlme_rx_enable_conf (uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-RX-ENABLE.confirm. More...
|
|
void | usr_mlme_scan_conf (uint8_t status, uint8_t ScanType, uint8_t ChannelPage, uint32_t UnscannedChannels, uint8_t ResultListSize, void *ResultList) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-SCAN.confirm. More...
|
|
void | usr_mlme_set_conf (uint8_t status, uint8_t PIBAttribute) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-SET.confirm. More...
|
|
void | usr_mlme_start_conf (uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-START.confirm. More...
|
|
void | usr_mlme_sync_loss_ind (uint8_t LossReason, uint16_t PANId, uint8_t LogicalChannel, uint8_t ChannelPage) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-SYNC-LOSS.indication. More...
|
|
retval_t | wpan_init (void) |
| The stack initialization function. More...
|
|
bool | wpan_mcps_data_req (uint8_t SrcAddrMode, wpan_addr_spec_t *DstAddrSpec, uint8_t msduLength, uint8_t *msdu, uint8_t msduHandle, uint8_t TxOptions) |
| Initiate MCPS-DATA.request service and have it placed in the MCPS-SAP queue. More...
|
|
bool | wpan_mcps_purge_req (const uint8_t msduHandle) |
| Initiate MCPS-PURGE.request service and have it placed in the MCPS-SAP queue. More...
|
|
bool | wpan_mlme_associate_req (uint8_t LogicalChannel, uint8_t ChannelPage, wpan_addr_spec_t *CoordAddrSpec, uint8_t CapabilityInformation) |
| Initiate MLME-ASSOCIATE.request service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_associate_resp (uint64_t DeviceAddress, uint16_t AssocShortAddress, uint8_t status) |
| Initiate MLME-ASSOCIATE.response service and place it in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_disassociate_req (wpan_addr_spec_t *DeviceAddrSpec, uint8_t DisassociateReason, bool TxIndirect) |
| Inititate MLME-DISASSOCIATE.request service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_get_req (uint8_t PIBAttribute) |
| Initiate MLME-GET.request service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_gts_req (uint16_t DevShortAddr, gts_char_t GtsChar) |
|
bool | wpan_mlme_orphan_resp (uint64_t OrphanAddress, uint16_t ShortAddress, bool AssociatedMember) |
| Initiate MLME-ORPHAN.response service and have it placed in MLME_SAP queue. More...
|
|
bool | wpan_mlme_poll_req (wpan_addr_spec_t *CoordAddrSpec) |
| Initiate MLME-POLL.request service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_reset_req (bool SetDefaultPib) |
| Initiate MLME-RESET.request service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_rx_enable_req (bool DeferPermit, uint32_t RxOnTime, uint32_t RxOnDuration) |
| Initiate MLME-RX-ENABLE.request service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_scan_req (uint8_t ScanType, uint32_t ScanChannels, uint8_t ScanDuration, uint8_t ChannelPage) |
| Initiate MLME-SCAN.request service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_set_req (uint8_t PIBAttribute, void *PIBAttributeValue) |
| Initiate MLME-SET.request service and have it placed in MLME_SAP queue. More...
|
|
bool | wpan_mlme_start_req (uint16_t PANId, uint8_t LogicalChannel, uint8_t ChannelPage, uint8_t BeaconOrder, uint8_t SuperframeOrder, bool PANCoordinator, bool BatteryLifeExtension, bool CoordRealignment) |
| Initiate MLME-START service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_mlme_sync_req (uint8_t LogicalChannel, uint8_t ChannelPage, bool TrackBeacon) |
| Initiate MLME-SYNC.request service and have it placed in the MLME-SAP queue. More...
|
|
bool | wpan_task (void) |
| The stack task function called by the application. More...
|
|