mlme_reset_conf_tag Struct Reference
MAC Data Structures
This is the MLME-RESET.confirm message structure.
#include <mac_msg_types.h>
Data Fields
enum
msg_code
cmdcode
< This identifies the message as
MLME_RESET_CONFIRM
More...
uint8_t
status
The result of the reset operation.
More...
Generated on Sat Mar 5 2022 00:34:19 for MAC No Beacon Application Device AT86RF233 (ATREB233-XPRO) - SAM4S Xplained Pro by
1.8.5