|
static float | calculate_net_data_rate (float per_test_duration_sec) |
| Function to calculate net data rate for the current PER test. More...
|
|
static float | calculate_time_duration (void) |
| Function to Calculate the time taken for PER Test. More...
|
|
uint8_t | check_error_conditions (void) |
| Function to check the error conditions before. More...
|
|
static void | config_ack_request (bool config_value) |
| To set or reset ACK request value. More...
|
|
static void | config_crc_peer_node (bool config_value) |
| To configure CRC settings on peer node. More...
|
|
static void | config_csma (bool config_value) |
| To configure CSMA Setting in the transceiver. More...
|
|
static void | config_frame_retry (bool config_value) |
| To configure frame retry Setting. More...
|
|
static void | config_rx_desensitization (bool config_value) |
| To configure rx desensitization level in the transceiver. More...
|
|
static void | configure_frame_sending (void) |
| To Configure the frame sending. More...
|
|
static void | configure_range_test_frame_sending (void) |
| To Configure the frame sending. More...
|
|
void | disconnect_peer_node (void) |
| Function to request the peer to get disconnected from source node. More...
|
|
| FLASH_DECLARE (uint8_t perf_config_param_size[]) |
|
void | get_board_details (void) |
| prints the hardware details More...
|
|
static void | get_crc_settings_peer_node (void) |
| Function used to query CRC settings in remote node. More...
|
|
void | get_current_configuration (void) |
| To Get the updated/latest values of all configurable parameters on source and peer node. More...
|
|
uint8_t | get_param_length (uint8_t parameter_type) |
|
void | get_sensor_data (void) |
| To get the Sensor data like Battery voltage. More...
|
|
void | identify_peer_node (void) |
| Identifying peer node. More...
|
|
void | initiate_per_test (void) |
| Initiates the test procedure. More...
|
|
void | initiate_range_test (void) |
| Initiates the Range test procedure. More...
|
|
void | per_mode_initiator_ed_end_cb (uint8_t energy_level) |
| User call back function after ED Scan completion. More...
|
|
void | per_mode_initiator_init (void *parameter) |
| Initialize the application in PER Measurement mode as Initiator. More...
|
|
void | per_mode_initiator_rx_cb (frame_info_t *frame) |
| Callback that is called if data has been received by trx in the PER_FOUND_PER_INITIATOR state. More...
|
|
void | per_mode_initiator_task (void) |
| Application task for PER Measurement mode as initiator. More...
|
|
void | per_mode_initiator_tx_done_cb (retval_t status, frame_info_t *frame) |
| Callback that is called once tx is done in the PER_FOUND_PER_INITIATOR state . More...
|
|
void | perf_get_req (uint8_t param_type_data) |
| Function to get the various configuaration paramters for PER Test. More...
|
|
void | perf_set_req (uint8_t set_param_type, param_value_t *param_value) |
|
More...
|
|
static void | range_test_timer_handler_cb (void *parameter) |
| This function is called periodically by the range test timer to initiate the transmission of range test packets to the receptor. More...
|
|
static bool | send_crc_set_req (crc_set_req_t crc_msg) |
| Function used to change CRC settings on peer node. More...
|
|
static bool | send_crc_status_req (void) |
| Function used to send crc status request to get CRC settings on the peer node. More...
|
|
static bool | send_disconnect_command (void) |
| Function used to send disconnect peer node command. More...
|
|
static bool | send_identify_command (void) |
| Function used to send identify peer node command. More...
|
|
static void | send_parameters_changed (uint8_t param, uint8_t val) |
| Function to send the parameters which has been updated to the receptor node. More...
|
|
static bool | send_peer_info_req (void) |
| Function to configure and send the peer node info request. More...
|
|
static bool | send_per_test_start_cmd (void) |
|
static bool | send_range_test_marker_rsp (void) |
| Function to send the response packet for the marker sent from the receptor. More...
|
|
static bool | send_range_test_start_cmd (void) |
| Function to send the range test start command to the receptor to start the mode in the receptor. More...
|
|
static bool | send_range_test_stop_cmd (void) |
| Function to send the range test stop command to the receptor to stop the mode in the receptor. More...
|
|
void | send_remote_cmd (uint8_t *serial_buf, uint8_t len, bool ack_req) |
| Function to send the command to Remote node to perform remote test. More...
|
|
static bool | send_result_req (void) |
| Function used to request PER test result. More...
|
|
static bool | send_set_default_config_command (void) |
| Function used to send set default config peer command. More...
|
|
static void | set_channel (uint16_t channel) |
| To set the Channel. More...
|
|
static void | set_channel_page (uint8_t channel_page) |
| To set the Channel Page. More...
|
|
void | set_default_configuration (void) |
| To set the default values of all configurable parameters on source and peer node. More...
|
|
static void | set_parameter_on_transmitter_node (retval_t status) |
| Set the parameters like channel,tx power etc on transmitter node. More...
|
|
static void | set_phy_frame_length (uint16_t frame_len) |
| To set PER Test frame length. More...
|
|
static void | set_transceiver_state (uint8_t trx_state) |
| Set Transceiver state as per the state given. More...
|
|
static void | set_tx_power (uint8_t tx_power_format, int8_t power_value) |
| To set the Tx power of the Transceiver. More...
|
|
void | start_ed_scan (uint8_t ed_scan_duration, uint32_t channel_sel_mask) |
| To start the ED scan. More...
|
|
static void | start_range_test (void) |
|
static void | start_test (void) |
|
void | stop_range_test (void) |
| Function to Stop the range Test in PER Mode. More...
|
|
static void | toggle_trx_sleep (void) |
| To toggle between sleep /deep state. More...
|
|
static void | wait_for_reply_timer_handler_cb (void *parameter) |
| Wait for reply timer handler is called if any command sent on air times out before any response message is received. More...
|
|