Initialization prototypes and enumerations - Performance Analyzer application.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include "tal.h"
#include "string.h"
#include "app_config.h"
#include "user_interface.h"
#include "conf_perf_analyzer.h"
Data Structures | |
struct | node_ib_t |
Structure to holds the information base for the node. More... | |
Macros | |
#define | CRC_SETTING_ON_REMOTE_NODE |
#define | DEFAULT_ADDR (0xFFFF) |
#define | DEFAULT_CHANNEL (11 + DEFAULT_CHANNEL_OFFSET) |
#define | DEFAULT_PAN_ID (0xCAFE) |
#define | DST_PAN_ID (DEFAULT_PAN_ID) |
#define | DST_SHORT_ADDR (0xFFFF) |
#define | DUMMY_PAYLOAD (0xAA) |
#define | FIRMWARE_VERSION 3.2 |
#define | FRAME_OVERHEAD (11) |
#define | FRAME_OVERHEAD_DST_IEEE_ADDR (FRAME_OVERHEAD + 6) |
#define | FRAME_OVERHEAD_SRC_IEEE_ADDR (FRAME_OVERHEAD + 6) |
#define | IC_TYPE 0X01 |
#define | LED_COUNT 0 |
#define | OFFSET_FOR_SRC_IEEE_ADDR (7) |
#define | SRC_PAN_ID (DEFAULT_PAN_ID) |
Functions | |
void | app_alert (void) |
void | config_node_ib (void) |
Function to init the information base for device. More... | |
void | init_state_init (void *arg) |
Initialization task for INIT STATE. More... | |
void | recover_all_settings (void) |
Recover all user settings before Start of CW transmission. More... | |
void | save_all_settings (void) |
Save all user settings before Start of CW transmission. More... | |
void | set_main_state (main_state_t state, void *arg) |
Function to set the main state of state machine. More... | |
retval_t | transmit_frame (uint8_t dst_addr_mode, uint8_t *dst_addr, uint8_t src_addr_mode, uint8_t msdu_handle, uint8_t *payload, uint16_t payload_length, uint8_t ack_req) |
Function to transmit frames as per 802.15.4 std. More... | |
void | wait_for_event_init (void *arg) |
Application task when the node is in the WAIT_FOR_EVENT state. More... | |
void | wait_for_event_rx_cb (frame_info_t *frame) |
Callback that is called if data has been received by trx in WAIT_FOR_EVENT state. More... | |
void | wait_for_event_task (void) |
Application task handling user events like key press or character on UART. More... | |
Variables | |
uint8_t | APP_TIMER_TO_RX_LED_OFF |
uint8_t | APP_TIMER_TO_TX |
uint8_t | APP_TIMER_TO_TX_LED_OFF |
uint8_t | CW_TX_TIMER |
volatile node_ib_t | node_info |
uint8_t | T_APP_TIMER |
uint8_t | T_APP_TIMER_RANGE |