Microchip® Advanced Software Framework

per_mode_receptor.c File Reference

Receptor functionalities in PER Measurement mode - Performance Analyzer application Copyright (c) 2013-2018 Microchip Technology Inc.

and its subsidiaries.

#include <stdio.h>
#include <stdlib.h>
#include <inttypes.h>
#include <ctype.h>
#include "app_init.h"
#include "tal_constants.h"
#include "tal_internal.h"
#include "tal_helper.h"
#include "ieee_const.h"
#include "app_frame_format.h"
#include "app_per_mode.h"
#include "conf_board.h"
#include "perf_api.h"
#include "led.h"

Macros

#define DELAY_BEFORE_APP_RESET_IN_MICRO_SEC   (5000)
 
#define LED_BLINK_COUNT_FOR_BUTTON_PRESS   (10)
 
#define LED_BLINK_RATE_IN_MICRO_SEC   (50000)
 

Functions

static void app_reset_cb (void *parameter)
 Timer Callback function if disconnect command is received on air by a node in reflector configuration.This is used to do a software reset on the reflector side. More...
 
static bool crc_check_ok (frame_info_t *mac_frame_info)
 Calculates CRC manually and compares with the received and returns true if both are same,false otherwise. More...
 
static uint16_t crc_test (uint16_t crc, uint8_t data)
 Calculates CRC for a given byte of data. More...
 
static void get_node_info (peer_info_rsp_t *data)
 Function used to get the board details of peer node. More...
 
void marker_rsp_timer_handler_cb (void *parameter)
 Timer Callback function if marker command is received on air This is used to blink the LED and thus identify that the marker frame is received. More...
 
void marker_tx_timer_handler_cb (void *parameter)
 Timer Callback function if marker response command is transmitted on air This is used to blink the LED and thus identify that the transmission is done. More...
 
void per_mode_receptor_init (void *parameter)
 Initialize the application in PER Measurement mode as Receptor. More...
 
void per_mode_receptor_rx_cb (frame_info_t *frame)
 Callback that is called if data has been received by trx in the PER_TEST_RECEPTOR state This call back is used when the node is operating as PER Measurement mode Receptor. More...
 
void per_mode_receptor_task (void)
 The application task when the node is in PER_TEST_RECEPTOR state i.e.PER Measurement mode as Receptor. More...
 
void per_mode_receptor_tx_done_cb (retval_t status, frame_info_t *frame)
 Callback that is called once tx is done in PER_TEST_RECEPTOR state This call back is used when the node is operating as PER Measurement mode Receptor. More...
 
static void send_crc_status_rsp (void)
 Function used to send crc settings on remote node to host node. More...
 
static void send_diversity_status_rsp (void)
 Function used to send diversity settings on remote node to host node. More...
 
static void send_peer_info_rsp (void)
 Function used to send peer_info_rsp command. More...
 
static bool send_range_test_marker_cmd (void)
 Function to send the range test marker command to the initiator node. More...
 
static void send_range_test_rsp (uint8_t seq_num, uint32_t frame_count, int8_t ed, uint8_t lqi)
 Function used to send response to the received range test packet. More...
 
bool send_remote_reply_cmd (uint8_t *serial_buf, uint8_t len)
 This function is used to send a remote test response command back to the initiator. More...
 
static void send_result_rsp (void)
 Function used to send PER test result. More...
 
static void set_paramter_on_recptor_node (app_payload_t *msg)
 Extract the received command frame and set the parameters like channel, tx power etc on Receptor node. More...
 

Variables

static uint32_t aver_lqi
 
static uint32_t aver_rssi
 
uint32_t frames_with_wrong_crc
 
bool manual_crc = false
 
static uint8_t marker_seq_num = 0
 
static uint32_t number_rx_frames
 
static bool range_test_in_progress = false
 
static uint8_t remote_cmd_len
 
static uint8_t * remote_cmd_ptr
 
static bool remote_cmd_rx = false
 
static uint8_t seq_num_receptor