|
bool | pal_calibrate_rc_osc (void) |
| Calibrates the internal RC oscillator. More...
|
|
void | pal_get_current_time (uint32_t *timer_count) |
| Gets current time. More...
|
|
retval_t | pal_init (void) |
| Initialization of PAL. More...
|
|
bool | pal_is_timer_running (uint8_t timer_id) |
| Checks if the timer of requested timer identifier is running. More...
|
|
void | pal_task (void) |
| Services timer and sio handler. More...
|
|
retval_t | pal_timer_get_id (uint8_t *timer_id) |
|
void | pal_timer_source_select (source_type_t source) |
| Selects timer clock source. More...
|
|
retval_t | pal_timer_start (uint8_t timer_id, uint32_t timer_count, timeout_type_t timeout_type, FUNC_PTR timer_cb, void *param_cb) |
| Start regular timer. More...
|
|
retval_t | pal_timer_stop (uint8_t timer_id) |
| Stops a running timer. More...
|
|
void | pal_trx_read_timestamp (uint32_t *timestamp) |
| Provides timestamp of the last received frame. More...
|
|