This is the MCPS-DATA.confirm message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
< This identifies the message as MCPS_DATA_CONFIRM More... | |
uint8_t | msduHandle |
The handle associated with the MSDU being confirmed. More... | |
uint8_t | status |
The status of the last MSDU transmission. More... | |