Microchip® Advanced Software Framework

tfa.h File Reference

This file is the interface for Transceiver Feature Access (TFA) functionality.

Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.

#include "return_val.h"
#include "ieee_const.h"
#include "tal_types.h"

Macros

#define SUPPLY_VOLTAGE_ABOVE_UPPER_LIMIT   (0xFFFF)
 Supply voltage above upper limit. More...
 
#define SUPPLY_VOLTAGE_BELOW_LOWER_LIMIT   (0)
 Supply voltage below lower limit. More...
 
#define TFA_PIB_RX_SENS_DEF   (RSSI_BASE_VAL_DBM)
 Default value of TFA PIB attribute to reduce the Rx sensitivity. More...
 

Typedefs

typedef enum continuous_tx_mode_tag continuous_tx_mode_t
 Continuous Transmission modes. More...
 
typedef enum tfa_pib_t tfa_pib_t
 Transceiver commands. More...
 

Enumerations

enum  continuous_tx_mode_tag {
  CW_MODE = 0,
  PRBS_MODE = 1
}
 Continuous Transmission modes. More...
 
enum  tfa_pib_t { TFA_PIB_RX_SENS = 0 }
 Transceiver commands. More...
 

Functions

retval_t tfa_batmon_irq_init (FUNC_PTR(batmon_irq_cb), uint16_t vth)
 Setups the battery monitor interrupt. More...
 
phy_enum_t tfa_cca_perform (void)
 Perform a CCA. More...
 
void tfa_continuous_tx_start (continuous_tx_mode_t tx_mode, bool random_content)
 Starts continuous transmission on current channel. More...
 
void tfa_continuous_tx_stop (void)
 Stops CW transmission. More...
 
uint8_t tfa_ed_sample (void)
 Perform a single ED measurement. More...
 
uint16_t tfa_get_batmon_voltage (void)
 Gets the transceiver's supply voltage. More...
 
double tfa_get_temperature (void)
 Get the temperature value from the integrated sensor. More...
 
retval_t tfa_init (void)
 Initializes the TFA. More...
 
retval_t tfa_pib_get (tfa_pib_t tfa_pib_attribute, void *value)
 Gets a TFA PIB attribute. More...
 
retval_t tfa_pib_set (tfa_pib_t tfa_pib_attribute, void *value)
 Sets a TFA PIB attribute. More...
 
void tfa_reset (bool set_default_pib)
 Reset the TFA. More...