Function prototypes for Peera Search process - Performance Analyzer application Copyright (c) 2013-2018 Microchip Technology Inc.
and its subsidiaries.
Data Structures | |
struct | peer_search_receptor_arg_t |
Structure to hold the peer device's short address and ieee address. More... | |
struct | peer_state_function_t |
Structure to hold the the function pointers to handle various Peer Search Process tasks. More... | |
Macros | |
#define | PEER_CONFIRM (0x03) |
#define | PEER_REQUEST (0x01) |
#define | PEER_RESPONSE (0x02) |
#define | PER_TEST_MODE (0x02) |
#define | RANGE_MEASURE_MODE (0x01) |
Functions | |
void | peer_search_initiator_exit (void) |
Function to exit peer search initiator exit state. More... | |
void | peer_search_initiator_init (void *arg) |
Application task to start peer search. More... | |
void | peer_search_initiator_rx_cb (frame_info_t *frame) |
Callback that is called if data has been received by trx. More... | |
void | peer_search_initiator_set_sub_state (uint8_t state, void *arg) |
Function to set the sub state of state machine. More... | |
void | peer_search_initiator_task (void) |
Application task handling peer search. More... | |
void | peer_search_initiator_tx_done_cb (retval_t status, frame_info_t *frame) |
Callback that is called once tx is done in peer search initiator state. More... | |
void | peer_search_receptor_exit (void) |
Function to exit peer search receptor state. More... | |
void | peer_search_receptor_init (void *arg) |
Application task to start peer search. More... | |
void | peer_search_receptor_rx_cb (frame_info_t *frame) |
Callback that is called if data has been received by trx in peer search receptor state. More... | |
void | peer_search_receptor_set_sub_state (uint8_t state, void *arg) |
Function to set the sub state of state machine. More... | |
void | peer_search_receptor_task (void) |
Application task handling peer search. More... | |
void | peer_search_receptor_tx_done_cb (retval_t status, frame_info_t *frame) |
Callback that is called once tx is done in peer search receptor state. More... | |