Microchip® Advanced Software Framework

range_measure.c File Reference

Range Measurement mode functionalities - Performance Analyzer application of AT86RF215 This implements the range measurement mode functionality.

Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdio.h>
#include <stdlib.h>
#include <inttypes.h>
#include <ctype.h>
#include "tal.h"
#include "tal_helper_2.h"
#include "app_init.h"
#include "ieee_const.h"
#include "app_frame_format.h"
#include "sio2host.h"
#include "app_range_mode.h"
#include "user_interface.h"

Macros

#define APP_SEND_TEST_PKT_INTERVAL_IN_MICRO_SEC   (250000)
 
#define DATA_PKT   (0x00)
 

Functions

void app_print_statistics (int trx)
 Print the statistics for Range Measurement on the UART Terminal. More...
 
static int range_test_frame_tx (void)
 Send Range Measurement mode test frames to the peer device. More...
 
void range_test_rx_cb (trx_id_t trx, frame_info_t *frame)
 Callback that is called if data has been received by trx when the node is in Range Measurement mode i.e RANGE_TEST_TX_ON or RANGE_TEST_TX_OFF. More...
 
void range_test_tx_off_task (trx_id_t trx)
 Application task handling Range Measurement when the node is in RANGE_TEST_TX_OFF state, where no TX is enabled and only RX is ON. More...
 
void range_test_tx_on_exit (trx_id_t trx)
 To exit the Application task from RANGE_TEST_TX_ON state, where both TX and RX is enabled. More...
 
void range_test_tx_on_init (trx_id_t trx, void *arg)
 Initialization of Range Measurement mode in RANGE_TX_ON State. More...
 
void range_test_tx_on_task (trx_id_t trx)
 Application task handling Range Measurement when the node is in RANGE_TEST_TX_ON state, where both TX and RX is enabled. More...
 
static void range_test_tx_timer_handler_cb (void *parameter)
 Callback function that handles timer in Range Measurement Mode. More...
 

Variables

static uint32_t num_of_frames_rec
 
static uint32_t num_of_frames_send
 
static uint8_t seq_num