Chip-specific system clock management functions.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
#include <compiler.h>
#include <stdbool.h>
#include <sysclk.h>
#include <avr32/io.h>
#include <flashc.h>
Macros | |
Initial module clock masks | |
These are the mask values written to the xxxMASK registers during initialization if the user has overridden the default behavior of all clocks left enabled. These values assume that:
| |
#define | SYSCLK_INIT_MINIMAL_CPUMASK |
Initial value of CPUMASK. More... | |
#define | SYSCLK_HSBMASK_STICKYBITS (0x00000800) |
Sticky Bits in HSBMASK according to the datasheet. More... | |
#define | SYSCLK_INIT_MINIMAL_HSBMASK |
Initial value of HSBMASK. More... | |
#define | SYSCLK_PBAMASK_STICKYBITS (0x00180000) |
Sticky Bits in PBAMASK according to the datasheet. More... | |
#define | SYSCLK_INIT_MINIMAL_PBAMASK |
Initial value of PBAMASK. More... | |
#define | SYSCLK_INIT_MINIMAL_PBBMASK 0 |
Initial value of PBBMASK. More... | |
Functions | |
void | sysclk_disable_usb (void) |
Disable the USB generic clock. More... | |
void | sysclk_enable_usb (void) |
Enable the USB generic clock. More... | |
void | sysclk_priv_disable_module (unsigned int bus_id, unsigned int module_index) |
Disable a maskable module clock. More... | |
void | sysclk_priv_enable_module (unsigned int bus_id, unsigned int module_index) |
Enable a maskable module clock. More... | |
Enabling and disabling synchronous clocks | |
void | sysclk_enable_pbb_module (unsigned int index) |
Enable a module clock derived from the PBB clock. More... | |
void | sysclk_disable_pbb_module (unsigned int index) |
Disable a module clock derived from the PBB clock. More... | |
System Clock Initialization | |
void | sysclk_init (void) |
Initialize the synchronous clock system. More... | |
Variables | |
static uint8_t | sysclk_bus_refcount [2] |
Number of enabled peripherals on the PBB and PBC busses. More... | |