FIFO descriptor used by FIFO driver.
#include <serial_fifo.h>
Data Fields | |
union { | |
uint16_t * ser_fifo_desc::u16ptr | |
Pointer to unsigned-16 bits location. More... | |
uint32_t * ser_fifo_desc::u32ptr | |
Pointer to unsigned-32 bits location. More... | |
uint8_t * ser_fifo_desc::u8ptr | |
Pointer to unsigned-8 bits location. More... | |
} | buffer |
uint16_t | mask |
Mask used to speed up FIFO operation (wrapping) More... | |
volatile uint16_t | read_index |
Read index. More... | |
uint16_t | size |
Size of the FIFO (unit is in number of 'element') More... | |
volatile uint16_t | write_index |
Write index. More... | |