Functions for manipulating Rime addresses
Functions | |
int | linkaddr_cmp (const linkaddr_t *addr1, const linkaddr_t *addr2) |
Compare two Rime addresses. More... | |
void | linkaddr_copy (linkaddr_t *dest, const linkaddr_t *from) |
Copy a Rime address. More... | |
void | linkaddr_set_node_addr (linkaddr_t *addr) |
Set the address of the current node. More... | |
Variables | |
linkaddr_t | linkaddr_node_addr |
The Rime address of the node. More... | |
const linkaddr_t | linkaddr_null = { { 0, 0, 0, 0, 0, 0, 0, 0 } } |
The null Rime address. More... | |