Microchip® Advanced Software Framework

list.h File Reference

Linked list manipulation routines.

Author
Adam Dunkels adam@.nosp@m.sics.nosp@m..se

Macros

#define LIST(name)
 Declare a linked list. More...
 
#define LIST_CONCAT(s1, s2)   LIST_CONCAT2(s1, s2)
 
#define LIST_CONCAT2(s1, s2)   s1##s2
 
#define LIST_STRUCT(name)
 Declare a linked list inside a structure declaraction. More...
 
#define LIST_STRUCT_INIT(struct_ptr, name)
 Initialize a linked list that is part of a structure. More...
 

Typedefs

typedef void ** list_t
 The linked list type. More...
 

Functions

void list_add (list_t list, void *item)
 Add an item at the end of a list. More...
 
void * list_chop (list_t list)
 Remove the last object on the list. More...
 
void list_copy (list_t dest, list_t src)
 Duplicate a list. More...
 
void * list_head (list_t list)
 Get a pointer to the first element of a list. More...
 
void list_init (list_t list)
 Initialize a list. More...
 
void list_insert (list_t list, void *previtem, void *newitem)
 Insert an item after a specified item on the list. More...
 
void * list_item_next (void *item)
 Get the next item following this item. More...
 
int list_length (list_t list)
 Get the length of a list. More...
 
void * list_pop (list_t list)
 Remove the first object on a list. More...
 
void list_push (list_t list, void *item)
 Add an item to the start of the list. More...
 
void list_remove (list_t list, void *item)
 Remove a specific element from a list. More...
 
void * list_tail (list_t list)
 Get the tail of a list. More...