uIP DNS resolver code header file.
#include "contiki.h"
Functions | |
CCIF void | mdns_conf (const uip_ipaddr_t *dnsserver) |
Configure a DNS server. More... | |
CCIF uip_ipaddr_t * | mdns_getserver (void) |
Obtain the currently configured DNS server. More... | |
void | mdns_init (void) |
CCIF uip_ipaddr_t * | mdns_lookup (const char *name) |
Look up a hostname in the array of known hostnames. More... | |
CCIF void | mdns_query (const char *name) |
Queues a name so that a question for the name will be sent out. More... | |
Variables | |
CCIF process_event_t | mdns_event_found |
Event that is broadcasted when a DNS name has been resolved. More... | |