In this section you can find all the projects related to the Clock Management.
Common API for Clocks Control / Example 1 for EVK1100 | |
Initialize the system clock and blink a LED at a constant 1Hz frequency. | |
Common API for Clocks Control / Example 1 for EVK1105 | |
Initialize the system clock and blink a LED at a constant 1Hz frequency. | |
Common API for Clocks Control / Example 2 for EVK1100 | |
Initialize the clock system and output the CPU clock on a dedicated pin. | |
Common API for Clocks Control / Example 2 for EVK1105 | |
Initialize the clock system and output the CPU clock on a dedicated pin. | |
Common API for Clocks Control / Example 3 for EVK1100 | |
Switch between various system clock sources and prescalers at run time. | |
Common API for Clocks Control / Example 3 for EVK1105 | |
Switch between various system clock sources and prescalers at run time. |
Basic clock service unit tests for EVK1100 | |
This is the unit tests of basic clock service. | |
Basic clock service unit tests for EVK1105 | |
This is the unit tests of basic clock service. |