In this section you can find all the projects related to the TWI - Two-Wire Interface.
TWI master Example for evk1100 | |
Using the TWI module in Master mode, perform read and write operation on a TWI slave. To be used with two boards with the corresponding Slave example. | |
TWI master Example for evk1105 | |
Using the TWI module in Master mode, perform read and write operation on a TWI slave. To be used with two boards with the corresponding Slave example. | |
TWI slave Example for evk1100 | |
Using the TWI module in Slave mode, process incoming read and write operations from/to a virtual memory space pre-allocated in internal RAM. To be used with two boards with the corresponding Master example. |