In this section you can find all the projects related to the MEMORY - DMACA - DMA Controller A.
DMACA RAM TO AES to ram Example 1 for EVK1104S | |
Using the DMACA, transfer data from RAM to AES then transfer the data back to the RAM. | |
DMACA RAM-to-RAM Example 2 for UC3-A3 Xplained | |
Using the DMACA, transfer data from RAM to RAM. | |
DMACA RAM_TO_RAM_EXAMPLE Example2 for evk1104 | |
Using the DMACA, transfer data from RAM to RAM. |