In this section you can find all the projects related to the MEMORY - ECCHRS - Error Corrected Code Controller.
ECCHRS Example for evk1104 | |
Using the ECCHRS, program an external Nand Flash block and write the corresponding ECC codewords, then read back the data and check if they are valid thanks to the ECC codewords. |