In this section you can find all the projects related to the TWI - Two-Wire Master Interface.
TWIM Master Example for evk1104 | |
Using the TWIM module, perform read and write operations from/to a virtual memory space pre-allocated in internal RAM in a slave TWI device. To be used with two boards with the corresponding TWIS module example. |