In this section you can find all the projects related to the CPU - PM - Power Manager.
PM Example1 for EVK1101 | |
Configure OSC0 as source of the main clock and configure a generic clock GCLK with OSC0 as input. Output the generic clock on a pin. Switch into the FROZEN sleep mode while still maintaining the generic clock output. | |
PM Example2 for EVK1101 | |
Configure a PLL (or a DFLL, depending on the device) and use it as the main clock source for the synchronous clocks. Configure a Generic Clock with the PLL (or DFLL) as input. Output the generic clock on a pin. |