Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an xTaskHandle variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 01:15:06 for UC3 B0/B1 by 1.8.5